Visible+IR in black and white mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Visible+IR in black and white mode

跳至解决方案
821 次查看
nav09
Contributor II

Hello, 

I am using IMX8M plus for my application development,

I have an 2MP RGB sensor with dual band pass filter lens (Visible+NIR 940nm), it outputs 12bit RAW RGB. Using IMX8M plus ISP, I need to fuse both visible and infrared (IR) data and convert into a single black and white (grayscale) image which can enhance imaging capabilities.

Is this supported in the IMX8Mplus ISP? how can I achieve this, which API should I use it?

Regards,

0 项奖励
回复
1 解答
671 次查看
nav09
Contributor II

Thanks, let me reach out to the local representative for the support on the tooling.

在原帖中查看解决方案

0 项奖励
回复
8 回复数
790 次查看
nav09
Contributor II

I understand this is not tested and guaranteed,

but is there an API available or any alternate solution available to convert into an grayscale Image, I can test this.

0 项奖励
回复
782 次查看
joanxie
NXP TechSupport
NXP TechSupport

I attached the AN for your reference, you can ty to use the tools to tune the ISP to check if it has the feature you need

0 项奖励
回复
772 次查看
nav09
Contributor II

I went through the reference document, basically there are two ways to tune to grayscale Image, tunning client is straight forward process with the documentation, 

I would be more interested to use tunning server i.e, to run directly on IMX8M plus , Is tunning client required as well?

or tunning server alone is sufficient, then with this 3 commands, can I convert into grayscaleImage?

root@cn-szh02-ns-pr002:~/all# systemctl stop weston*
root@cn-szh02-ns-pr002:~/all# chmod 777 tuningext
root@cn-szh02-ns-pr002:~/all# ./tuningext&

 

0 项奖励
回复
725 次查看
joanxie
NXP TechSupport
NXP TechSupport

you should use tuning tool to support this,  for tuning tool,  you need contact local representative to get it 

0 项奖励
回复
697 次查看
nav09
Contributor II

Yes, the tunning tool is required and I can request the local representative.

but, Is that for tunning server I need to request for, I need to convert this onchip an not offline (tunning client)?

0 项奖励
回复
684 次查看
joanxie
NXP TechSupport
NXP TechSupport

I don't have tuning tool so I didn't use tuning server before, since you need to request this tool, you can test after you get this tools, as my understanding, after you build the ISP sdk, you would get the library files, then you can use the tuning server by these library files

0 项奖励
回复
672 次查看
nav09
Contributor II

Thanks, let me reach out to the local representative for the support on the tooling.

0 项奖励
回复
793 次查看
joanxie
NXP TechSupport
NXP TechSupport

this is my another case, I confirmed that we couldn't guarantee this because we don't test this yet

Solved: MX8MP ISP with IR wavelengths - NXP Community

0 项奖励
回复