Visible+IR in black and white mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Visible+IR in black and white mode

ソリューションへジャンプ
772件の閲覧回数
nav09
Contributor II

Hello, 

I am using IMX8M plus for my application development,

I have an 2MP RGB sensor with dual band pass filter lens (Visible+NIR 940nm), it outputs 12bit RAW RGB. Using IMX8M plus ISP, I need to fuse both visible and infrared (IR) data and convert into a single black and white (grayscale) image which can enhance imaging capabilities.

Is this supported in the IMX8Mplus ISP? how can I achieve this, which API should I use it?

Regards,

ラベル(1)
0 件の賞賛
返信
1 解決策
622件の閲覧回数
nav09
Contributor II

Thanks, let me reach out to the local representative for the support on the tooling.

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
741件の閲覧回数
nav09
Contributor II

I understand this is not tested and guaranteed,

but is there an API available or any alternate solution available to convert into an grayscale Image, I can test this.

0 件の賞賛
返信
733件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I attached the AN for your reference, you can ty to use the tools to tune the ISP to check if it has the feature you need

0 件の賞賛
返信
723件の閲覧回数
nav09
Contributor II

I went through the reference document, basically there are two ways to tune to grayscale Image, tunning client is straight forward process with the documentation, 

I would be more interested to use tunning server i.e, to run directly on IMX8M plus , Is tunning client required as well?

or tunning server alone is sufficient, then with this 3 commands, can I convert into grayscaleImage?

root@cn-szh02-ns-pr002:~/all# systemctl stop weston*
root@cn-szh02-ns-pr002:~/all# chmod 777 tuningext
root@cn-szh02-ns-pr002:~/all# ./tuningext&

 

0 件の賞賛
返信
676件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

you should use tuning tool to support this,  for tuning tool,  you need contact local representative to get it 

0 件の賞賛
返信
648件の閲覧回数
nav09
Contributor II

Yes, the tunning tool is required and I can request the local representative.

but, Is that for tunning server I need to request for, I need to convert this onchip an not offline (tunning client)?

0 件の賞賛
返信
635件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I don't have tuning tool so I didn't use tuning server before, since you need to request this tool, you can test after you get this tools, as my understanding, after you build the ISP sdk, you would get the library files, then you can use the tuning server by these library files

0 件の賞賛
返信
623件の閲覧回数
nav09
Contributor II

Thanks, let me reach out to the local representative for the support on the tooling.

0 件の賞賛
返信
744件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

this is my another case, I confirmed that we couldn't guarantee this because we don't test this yet

Solved: MX8MP ISP with IR wavelengths - NXP Community

0 件の賞賛
返信