Hi community,
I have an unwanted periodic noise on output audio on a imx6 dual lite based board.
The setup is the following:
rootfs built with yocto master-next, image based on fsl-image-multimedia, and linux kernel is 3.10.31 BETA.
I tried to play an audio file with two methods:
- with aplay
- and with gstreamer0.10
In two cases, I had a periodic noise which happen on output audio after about 45 minutes. Is it a driver problem?
Do you have solution?
Regards,
Jordan
Hi jordan
beta releases are not fully tested, please try latest dizzy or 3.10.53 :
http://freescale.github.io/doc/release-notes/1.7/index.html
L3.10.53_1.1.0_iMX6QDLS_Bundle : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,
i.MX 6Solo Linux Binary Demo Files and Linux BSP Documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
For others reasons, I must use this beta release.
Do you have others solutions, please?
Regards,
Jordan
Hi,
For my part, I don't find solutions for this audio problem. Do you have solutions?
regards,
Jordan
Hi,
I tried with daisy release and I have the same problem.
Do you have solution, please?
Jordan
Hi,
An additional information:
I play song on HDMI output.
Regards,
Jordan