Unable to play videos on QML Qt6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to play videos on QML Qt6

Jump to solution
2,030 Views
imahgin
Contributor III

Hi,

I've developed a QML app on an iMX93 platform (Yocto + Qt6.4) and I'm experiencing an issue when trying to play videos.
Whether I use MediaPlayer + VideoOutput or Video components, I'm not able to view anything on the screen. Audio plays ok though

This is a snippet of my code, but video QML examples also doesn't work.

    Video {
        id: video
        anchors.fill: parent
        source: "file:///home/root/turning_pages.avi"
        fillMode: Image.Stretch
        muted: false

        Component.onCompleted: play()

        onErrorOccurred: error => console.log('Error occurred:', errorString, error)
        onPlaying: console.log('playing stream', source)
        onStopped: console.log('stream stopped')
        onBufferProgressChanged: console.log('buffering:', bufferProgress)
    }

And this is the console output -no warnings nor errors-

====== AIUR: 4.7.3 build on Feb  3 2023 05:14:46. ======
	Core: AVI_PARSER_03.06.08  build on Sep 26 2022 08:17:20
 file: /usr/lib/imx-mm/parser/lib_avi_parser_arm_elinux.so.3.1
------------------------
    Track 00 [video_0] Enabled
	Duration: 0:00:15.533178000
	Language: und
    Mime:
	image/jpeg, width=(int)160, height=(int)120, framerate=(fraction)500000/33333 
------------------------
------------------------
    Track 01 [audio_0] Enabled
	Duration: 0:00:15.533381000
	Language: und
    Mime:
	audio/x-raw, format=(string)U8, channels=(int)1, layout=(string)interleaved, rate=(int)11024, bitrate=(int)88192 

I'm able to play the video using gst-launch

gst-launch-1.0 playbin uri=file:///home/root/turning_pages.avi video-sink="waylandsink sync=false"

So it seems it's not a codec related issue, but these are the gstreamer plugins installed:

 

CORE_IMAGE_EXTRA_INSTALL += "gstreamer1.0-plugins-ugly-meta packagegroup-fsl-gstreamer1.0-commercial"  

LICENSE_FLAGS_ACCEPTED += "commercial"  

CORE_IMAGE_EXTRA_INSTALL += " \  
 packagegroup-fsl-tools-gpu \  
 packagegroup-fsl-gstreamer1.0 \  
 packagegroup-fsl-gstreamer1.0-full \  
" 

 

Running Qt widgets examples does works and both video and audio works fine, so it seems only related to the QML side

When building Yocto I've also added the following lines:

IMAGE_INSTALL:append = " qtmultimedia qtmultimedia-plugins qtmultimedia-qmlplugins"

PACKAGECONFIG:append_pn-qtmultimedia = " gstreamer gstreamer010"
"

Thks in advance

0 Kudos
1 Solution
1,274 Views
imahgin
Contributor III

Today I've received the latest i.MX93 SOC version and compiled again Yocto with the latest BSP, and finally the QML streaming issue is fixed!!!

So, in my case was a SOC version problem.

View solution in original post

0 Kudos
11 Replies
971 Views
wooosaiiii
Contributor III

@imahgin Can you confirm you are using i.MX93 rev=A1 + Qt6 + QML to play videos? 

0 Kudos
945 Views
imahgin
Contributor III

Yeap, but this lead to an unexpected performance issue as all animations in QML run very slowly making the app unusable.

Reverting some commits fixes this issue, but then, the Video is broken again.

Looks like switching to linuxfb -required because iMX93 has no GPU- somehow break Qt multimedia framework

 

0 Kudos
1,275 Views
imahgin
Contributor III

Today I've received the latest i.MX93 SOC version and compiled again Yocto with the latest BSP, and finally the QML streaming issue is fixed!!!

So, in my case was a SOC version problem.

0 Kudos
1,300 Views
imahgin
Contributor III

I opened a case in NXP and the good news is that they are aware of the problem and it'll eventually be fixed in upcoming releases.
According to their response, the issue is related to libqt6-qtlocation ¿?

The problem is that new releases are only compatible with the latest i.MX93 SOC

 

BR

0 Kudos
1,694 Views
imahgin
Contributor III

I found this patch to provide Qt6 option for qmlgl.

For testing purposes, instead of creating my own layer, I directly modified gstreamer1.0-plugins-good_1.22.0.imx.bb -and also gstreamer1.0-plugins-good_1.22.0.bb just in case- with that patch

QTWAYLANDDEPENDS = "${@bb.utils.contains("DISTRO_FEATURES", "wayland", "qtwayland", "", d)}"  

 

PACKAGECONFIG[qt5]        = "-Dqt5=enabled,-Dqt5=disabled,qtbase qtdeclarative qtbase-native ${QTWAYLANDDEPENDS}" 
PACKAGECONFIG[qt6]        = "-Dqt6=enabled,-Dqt6=disabled,qtbase qtdeclarative qtbase-native qttools-native ${QTWAYLANDDEPENDS}" 

 

do_configure:prepend() { 

    # provide path to qtwaylandscanner 

    export PATH=${PATH}:${STAGING_DIR_NATIVE}/${libexecdir} 

} 

Yocto build succeeded but 2 warnings are issued

WARNING: gstreamer1.0-plugins-good-1.22.0.imx-r0 do_configure: QA Issue: gstreamer1.0-plugins-good: invalid PACKAGECONFIG: qmlglsink [invalid-packageconfig]
WARNING: gstreamer1.0-plugins-good-1.22.0.imx-r0 do_configure: QA Issue: gstreamer1.0-plugins-good: invalid PACKAGECONFIG: qmlglsrc [invalid-packageconfig]

And the plugins, obviously, are missing in the Yocto compilation.

What I'm missing here?

0 Kudos
1,784 Views
imahgin
Contributor III

I made some modifications to my local.conf trying to include the QML plugins:


IMAGE_INSTALL:append = " qtmultimedia qtmultimedia-plugins qtmultimedia-qmlplugins" VIDEO_TOOLS = " \ gstreamer1.0 \ gstreamer1.0-plugins-good \ gstreamer1.0-plugins-base \ gstreamer1.0-plugins-ugly \ gstreamer1.0-libav \ gst-player \ gstreamer1.0-meta-base \ gst-examples \ gstreamer1.0-rtsp-server \ " IMAGE_INSTALL:append = " ${VIDEO_TOOLS}" LICENSE_FLAGS_ACCEPTED += "commercial"
PACKAGECONFIG:append:pn-gstreamer1.0-plugins-good = " qmlglsink"
PACKAGECONFIG:append:pn-gstreamer1.0-plugins-good = " qmlglsrc"
PACKAGECONFIG:append:pn-qtmultimedia = " gstreamer qml"

But again I have no QML plugins installed when building Yocto.

How can I instruct bitbake to include gstreamer QML plugins in my compilation?

0 Kudos
1,847 Views
imahgin
Contributor III

According to the i.MX Linux Release Notes Rev. LF6.1.22_2.0.0, Gstreamer has been upgraded to 1.22.0!!!
I've built a new Yocto image based on mx93-yocto-mickledore-6.1.22_2.0.0-v1.0 and checked that gstreamer version is really 1.22.0, but still cannot play video -sound works fine- and no errors are displayed on console.

0 Kudos
1,904 Views
imahgin
Contributor III

According to this information seems that Qt6 support for rendering video inside a QML scene is available only from version 1.22.0, and according to this document this version is included in Rev. LF6.1.36_2.1.0 (page 9)

My distribution has 1.20.3. As I'm not an experienced user in Yocto, is there any 'easy' way to include this -or latest version- on our current Yocto compilation, without breaking other packages?

 

Thks

0 Kudos
1,930 Views
imahgin
Contributor III

Some updates from my part.

I've compiled a Dunfell distribution -based on Qt5- and everything works fine out of the box.

Didn't install any additional codec and video plays fine from both command line and QML app.

It looks like it's only related to the compiled Multimedia component on embedded Qt6

Any other clue?

0 Kudos
2,002 Views
brian14
NXP TechSupport
NXP TechSupport

Hi @imahgin

Thank you for contacting NXP Support.

You can try using the Gstreamer pipeline in your QML code.

Here is an example:

Gstreamer in command line pipeline:

$ gst-launch-1.0 -e filesrc location=video.mp4 ! qtdemux ! h264parse ! v4l2h264dec ! imxvideoconvert_g2d ! queue ! waylandsink

Gstreamer pipeline used in QML code:

source : "gst-pipeline: filesrc location=/home/root/video.mp4 ! qtdemux ! h264parse ! v4l2h264dec ! imxvideoconvert_g2d ! qtvideosink"

I hope this information will helpful.

1,989 Views
imahgin
Contributor III

Hi @brian14

Thks for the suggestion but I've already tried a pipeline (using qmlglsink on avi file), but neither of them works in QML

The following message is displayed on console:

qt.multimedia.player: Unable to set the pipeline to the paused state.

If running gst-launch, then some components are missed

erroneous pipeline: no element "v4l2h264dec"
erroneous pipeline: no element "imxvideoconvert_g2d"
erroneous pipeline: could not link queue0 to waylandsink0

but the following do works:

gst-launch-1.0 playbin uri=file:///home/root/video.mp4 video-sink="waylandsink sync=false"

so I guess some codecs are missed in my Yocto project.

I had no issues using Qt5 without using pipelines, so I'll dig deeper into my Yocto compilation.

0 Kudos