Unable to give Keyboard input for IMX8QM-MEK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to give Keyboard input for IMX8QM-MEK

306件の閲覧回数
LokeshGandham
Contributor I

I have downloaded the pre-built Linux image from here  and flashed the SD card with 

```

sudo dd if=imx-image-full-imx8qmmek.wic of=/dev/sdc bs=1M && sync

``` 

 I was able to see imx8qmmek login prompt in minicom terminal but unable to give any keyboard input for logging in. attached the screenshot and bootup logs.

ラベル(2)
0 件の賞賛
1 返信

287件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport


Hi @LokeshGandham!
Thank you for contacting NXP Support!

Try to run minicom with sudo.

If the problem persists, try to use "screen" instead of minicom, and change the USB debug cable if necessary.

The board is booting correctly, I think is a Host issue.

Best Regards!

Chavira

0 件の賞賛