Uboot splash screen is not enough, info for kernel bootsplash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Uboot splash screen is not enough, info for kernel bootsplash

跳至解决方案
1,464 次查看
mirogliopaolo
Contributor II

I'm using the u-boot bootsplash but is lousy as no kernel loading iteraction is possible:

-no loading scrolling bar

-boot console must be totally hidden or totally shown

On x86 systems i used some years ago a bootsplash composed by scripts and kernel driver, it worked perfectly, because it was possible to press ESC key to show the underlying console and also to send to /dev/splash a message or the progressbar status.

Somebody is using similar system?

If not i will try a porting of that (it was running on LFS).

Best Regards

Miroglio

标签 (4)
标记 (3)
0 项奖励
回复
1 解答
1,166 次查看
juangutierrez
NXP Employee
NXP Employee

These features are provided by a separate splashutils package which is a set of userspace scripts and kernel patches, however this package is not maintained by FSL.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,167 次查看
juangutierrez
NXP Employee
NXP Employee

These features are provided by a separate splashutils package which is a set of userspace scripts and kernel patches, however this package is not maintained by FSL.

0 项奖励
回复
1,166 次查看
mirogliopaolo
Contributor II

Dear Juan,

thank you very much for the answer, that's what i was looking for!

Regards

Miroglio Paolo

0 项奖励
回复