USB OTG on IMX6DL detection problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB OTG on IMX6DL detection problem

3,447 Views
enricorossi
Contributor I

Dear All,

I am using an IMX6DL on a custom board and I am trying to use the USB OTG interface. I am currently facing some problems regarding the interface detection.

In particular, I have no information about the OTG interface on the dmesg kernel log and, even if I am sure the OTG Vbus power is on (thanks to led DL6), Linux is not able to detect any usb peripheral.

In the following you can find all the information about the schematic, the devicetree and kernel configuration.

- Schematic:

Screenshot from 2018-03-16 14-04-17.png

Signal connection to the processor:

Signal Name                  Processor pin            Pin Muxing

USB_OTG_N                  B6                               (this pin has no alternate functions)

USB_OTG_P                  A6                               (this pin has no alternate functions)

USB_OTG_ID                 W23                            GPIO1_24

USB_OTG_H1_OC         J20                             GPIO3_30

USB_OTG_PWR_EN      V5                              GPIO4_15

USB_OTG_OC                T6                              GPIO4_14

- Device Tree

In the following the otg part in the .dts file.

&usbotg {
      status = "okay";
      dr_mode = "otg";
      srp-disable;
      hnp-disable;
      adp-disable;
      disable-over-current;
};

I have also tried to remove the options srp-disable, hnp-disable, and adp-disable without any success.

In the following the otg part of the .dtsi file.

pinctrl_usbotg: usbotggrp {
      fsl,pins = <
      MX6QDL_PAD_KEY_COL4__USB_OTG_OC 0x1b0b0 
      MX6QDL_PAD_ENET_RX_ER__USB_OTG_ID 0x1b0b0
      >;

};

pinctrl_usbotg_vbus: usbotg_vbusgrp {
      fsl,pins = <
      /* power enable, low active */
      #define GP_USB_OTG_PWR <&gpio4 15 GPIO_ACTIVE_LOW>
      MX6QDL_PAD_KEY_ROW4__GPIO4_IO15 0x17059
      >;
};

reg_usbotg_vbus: regulator@4 {
      compatible = "regulator-fixed";
      reg = <4>;
      pinctrl-names = "default";
      pinctrl-0 = <&pinctrl_usbotg_vbus>;
      regulator-name = "usbotg_vbus";
      regulator-min-microvolt = <5000000>;
      regulator-max-microvolt = <5000000>;
      gpio = GP_USB_OTG_PWR;
      enable-active-low;
};

&usbotg {
      vbus-supply = <&reg_usbotg_vbus>;
      pinctrl-names = "default";
      pinctrl-0 = <&pinctrl_usbotg>;
      disable-over-current;
      status = "okay";
};

- Kernel

Regarding the loaded kernel modules, I followed the IMX6 reference manuale (https://nxpcommunity.force.com/sfc/servlet.shepherd/document/download/06957000004mHAWAA2?operationCo..., section 39.3.3, page 316) and I loaded the following modules:

1. CONFIG_USB - Build Support for Host-side USB
2. CONFIG_USB_EHCI_HCD - EHCI HCD (USB 2.0) support
3. CONFIG_USB_CHIPIDEA - ChipIdea high-speed Dual Role Controller
4. CONFIG_USB_CHIPIDEA_UDC - ChipIdea device controller
5. CONFIG_USB_CHIPIDEA_HOST - ChipIdea host controller
6. CONFIG_USB_GADGET - USB Gadget Support
7. CONFIG_USB_MXS_PHY - Freescale MXS USB PHY support

Note that module 6 has been loaded manually after system boot.

Am I doing something wrong? Can you please give me some support?

Thanks and best regards,

Enrico

Labels (1)
0 Kudos
Reply
2 Replies

2,344 Views
enricorossi
Contributor I

Hi igorpadykov‌,

Thank you for your answer. I checked the documents you sent me and I found a hardware problem on the board.

Kernel configuration and device tree were good.

Regards,

Enrico

0 Kudos
Reply

2,344 Views
igorpadykov
NXP Employee
NXP Employee

Hi Enrico

one can check VDD_VBUS_CAP described in Figure 51-1. Power system overview

i.MX6SDL Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

check 24MHz crystal, probably replacing from working board. Use Chapter 6
Avoiding Board Bring-up Problems i.MX6 System DevelopmentUser’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

May be recommended to test usb in uboot or with bare metal SDK:

Github SDK
https://github.com/backenklee/swp-report/tree/master/iMX6_Platform_SDK

Also simple way to test usb with mfg tool - if it detects board, can be found on

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply