Trouble booting imx25 3 stack board with latest u-boot 2014.10 u-boot.bin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trouble booting imx25 3 stack board with latest u-boot 2014.10 u-boot.bin

727件の閲覧回数
madhurabhashini
Contributor II

Hi,

I downloaded the latest u-boot source from http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/log/?h=imx_v2014.04_3.10.31_1.1.0_beta2

I built u-boot by following:

export ARCH=arm

export CROSS_COMPILE=arm-linux-gnueabi

make mx25pdk_config

make

This generates u-boot.bin and u-boot.imx.

I understand that u-boot.imx works with internal boot mode(secure mode). But my imx 25 3 stack board is in external direct boot. I tried to boot up the board using NAND and SD card with u-boot.bin, but in vain. Kindly let me know what should be done.

However I am able to build u-boot.2009.08 using ltib and the u-boot/kernel source available freescale community downloads.

Also, would like to know the difference between imx25_3stack folder structure in u-boot 2009.08 releases and mx25pdk_config folder in latest u-boot releases u-boot.2014.10.

Thanks in advance!

Madhura

ラベル(1)
タグ(4)
0 件の賞賛
1 返信

344件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Madhurabhashini

beta releases may not be fully tested, so I would suggest to wait

for final. Boot modes selection (internal and external) is described in

attached file p.12. As for Uboot 2009 vs 2014 internal structure differencies

please post on Uboot forum

WebHome < U-Boot < DENX

Best regards

igor

0 件の賞賛