What is the TOPS of the MIMX8DL1AVNFZAB? We cannot find it from datasheets and Factor sheets.
Please help to check it.
thanks
Yes.It would be ok for TOPS of GPU.Would you please help tp share it ?thanks.
this is not official test result, just for reference
Here is the test result from internal team on i.MX8QXP MEK board. (8DX use the same GPU as 8QXP)
root@imx8qxpmek:~# ./clpeak
Platform: Vivante OpenCL Platform
Device: Vivante OpenCL Device GC7000L.6214.0000
Driver version : OpenCL 1.2 V6.2.4.p4.190076 (Linux ARM64)
Compute units : 1
Clock frequency : 850 MHz
Global memory bandwidth (GBPS)
float : 2.75
float2 : 5.07
float4 : 6.90
float8 : 5.77
float16 : 4.07
Single-precision compute (GFLOPS)
float : 6.63
float2 : 13.53
float4 : 26.88
float8 : 26.63
float16 : 26.41
No half precision support! Skipped
No double precision support! Skipped
Integer compute (GIOPS)
int : 6.79
int2 : 6.78
int4 : 6.77
int8 : 6.72
int16 : 6.70
Transfer bandwidth (GBPS)
enqueueWriteBuffer : 1.64
enqueueReadBuffer : 0.09
enqueueMapBuffer(for read) : 273.58
memcpy from mapped ptr : 0.09
enqueueUnmap(after write) : 228.22
memcpy to mapped ptr : 1.65
Kernel launch latency : 96.73 us