Hi Team,
also we need following path to locate external storage (SDCARD) in adb shell:
Currently it is points to the internal memory which is android file system.
We need /sdcard path as a /sdcard/<Sdcard_name_byUser>
Thanks
Divyesh
Hi @joanxie ,
We have added support for exfat in Android 11 code base. Now exfat formatted SDcard is supporting.
But we are not able to create folder in /sdcard folder. We need External sdcard points to the /sdcard/ClubCar directory. But in current implementation it is pointing to internal storage of device. need to change path to point External sdcard. Could you please help here ?
Thanks
Hi @joanxie ,
I tried to format SDcard with exfat and it is working through adb shell :
evk_8mm:/ # mkfs.exfat /dev/block/mmcblk1p1
mkexfatfs 1.3.0
Creating... done.
Flushing... done.
File system created successfully.
After executing these commands, I can see type=exfat.
BUT I need default format exfat without any commands through adb shell...