Show ## Auxiliary core is already up when run m4boot_0 in boot command line

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Show ## Auxiliary core is already up when run m4boot_0 in boot command line

738 次查看
wang12zhe
Contributor III

HW:IMX8QM MEK

Yocto: L5.10.52

When I try to run m4boot_0  in uboot ,I got below output:

=> run m4boot_0
8664 bytes read in 4 ms (2.1 MiB/s)
## Auxiliary core is already up
=>

I can't find any output after run m4boot_0 , So I think M4 firmware not start, 

How start M4 firmware when run   m4boot_0  ?

 

 

 

0 项奖励
回复
1 回复

692 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @wang12zhe !


The iMX8QM has a different way of getting up the M core.

Please check our "Getting started with MCUXpresso" in chapter 6.1 "!Run an example application on one of the two M4 cores" and "Linux User guide" in chapter 4.5.13 "How to build imx-boot image by using imx-mkimage" in those chapters explains how to build and image for the board an run your code on the
M core

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf


Best Regards!
Chavira

0 项奖励
回复