Hi everyone,
I'm trying to update from Linux 4.1 (Yocto Krogoth) to 4.9 (Yocto Sumo) using a iMX6UL. Everything is working fine but I'm not able to use a DAC and ADC both connected to SAI1. In Linux 4.1 there was no problem. Unfortunately in 4.9 a got this message "Trying to bind component to card X but is already bound to card Y", just DAC card is declared after that and works fine using GStreamer or ALSA. Then, I patched soc-core.c to avoid launch this error and both cards finally appear in the list of declared sound cards. But now, when I try to play a sine using GStreamer, I get message "Setting pipeline to PAUSED ..." and cannot kill the process...
I was wondering if with the current kernel drivers is possible to define more than one sound card for the same sai.
Thanks
已解决! 转到解答。
I've solved by defining a sound card with 2 codecs:
sound-10 {
compatible = "simple-audio-card";
simple-audio-card,name = "10_audio";
system-clock-direction = "out";
system-clock-type = "mclk";
simple-audio-card,dai-link@0{
format = "i2s";
cpu {
sound-dai = <&sai1>;
dai-tdm-slot-num = <2>;
system-clock-frequency = <12288000>;
};
codec {
sound-dai = <&codec1>;
system-clock-id = <2>;
system-clock-frequency = <12288000>;
};
};
simple-audio-card,dai-link@1{
format = "i2s";
cpu {
sound-dai = <&sai1>;
dai-tdm-slot-num = <2>;
system-clock-frequency = <12288000>;
};
codec {
sound-dai = <&codec2>;
system-clock-id = <2>;
system-clock-frequency = <12288000>;
};
};
};
Is not necessary to patch soc-core file.
Hi @stefanozuincast ,
i want btsco codec and wm8960 codec drivers to use sai2 interface.
i tried adding the dts nodes as you mentioned. its building fine and android booted up but no codec soundcards were created.
mentioning the node :
sound-new {
compatible = "simple-audio-card";
simple-audio-card,name = "mixcard";
simple-audio-card,dai-link@0{
simple-audio-card,format = "i2s";
simple-audio-card,bitclock-master = <&dailink_master>;
simple-audio-card,frame-master = <&dailink_master>;
simple-audio-card,mclk-fs = <32>;
simple-audio-card,widgets =
"Microphone", "Mic Jack",
"Line", "Line In",
"Line", "Line Out",
"Speaker", "Speaker",
"Headphone", "Headphone Jack";
simple-audio-card,routing =
"Headphone Jack", "HP_L",
"Headphone Jack", "HP_R",
"Speaker", "SPK_LP",
"Speaker", "SPK_LN",
"LINPUT1", "Mic Jack",
"LINPUT3", "Mic Jack",
"RINPUT1", "Mic Jack",
"RINPUT2", "Mic Jack";
status = "okay";
dailink_master: simple-audio-card,cpu {
sound-dai = <&sai2>;
};
simple-audio-card,codec {
sound-dai = <&codec>;
system-clock-frequency = <12288000>;
};
};
simple-audio-card,dai-link@1{
simple-audio-card,format = "i2s";
simple-audio-card,bitclock-inversion;
simple-audio-card,frame-master = <&btcpu>;
simple-audio-card,bitclock-master = <&btcpu>;
btcpu: simple-audio-card,cpu {
sound-dai = <&sai2>;
dai-tdm-slot-num = <2>;
dai-tdm-slot-width = <16>;
};
simple-audio-card,codec {
sound-dai = <&bt_sco_codec 0>;
};
};
};
please help here @igorpadykov
I've solved by defining a sound card with 2 codecs:
sound-10 {
compatible = "simple-audio-card";
simple-audio-card,name = "10_audio";
system-clock-direction = "out";
system-clock-type = "mclk";
simple-audio-card,dai-link@0{
format = "i2s";
cpu {
sound-dai = <&sai1>;
dai-tdm-slot-num = <2>;
system-clock-frequency = <12288000>;
};
codec {
sound-dai = <&codec1>;
system-clock-id = <2>;
system-clock-frequency = <12288000>;
};
};
simple-audio-card,dai-link@1{
format = "i2s";
cpu {
sound-dai = <&sai1>;
dai-tdm-slot-num = <2>;
system-clock-frequency = <12288000>;
};
codec {
sound-dai = <&codec2>;
system-clock-id = <2>;
system-clock-frequency = <12288000>;
};
};
};
Is not necessary to patch soc-core file.
Hi Stefano
one can try with nxp linux releases: L4.9.88 (rocko)
https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.88_2.0.0_ga
or L4.14.78 (sumo)
https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.14.78_1.0.0_ga
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
I'm currently using Linux Kernel 4.9.88 and I get that error...
This is my audio codecs declaration:
/ {
sound-dac {
compatible = "simple-audio-card";
simple-audio-card,name = "pcm179x-audio";
simple-audio-card,format = "i2s";
system-clock-direction = "out";
system-clock-type = "mclk";
simple-audio-card,cpu {
sound-dai = <&sai1>;
};
dailink_master: simple-audio-card,codec {
sound-dai = <&codec1>;
system-clock-id = <2>;
system-clock-frequency = <12288000>;
};
};
sound-adc {
compatible = "simple-audio-card";
simple-audio-card,name = "pcm186x-audio";
simple-audio-card,format = "i2s";
system-clock-direction = "out";
system-clock-type = "mclk";
simple-audio-card,cpu {
sound-dai = <&sai1>;
};
dailink_master: simple-audio-card,codec {
sound-dai = <&codec2>;
system-clock-id = <2>;
system-clock-frequency = <12288000>;
};
};
};
&i2c4 {
clock_frequency = <400000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c4>;
status = "okay";
codec1: pcm1796@4c {
#sound-dai-cells = <0>;
compatible = "ti,pcm179x";
reg = <0x4c>;
clocks = <&clks IMX6UL_CLK_SAI1>;
clock-names = "mclk";
};
codec2: pcm1864@4a {
reg = <0x4a>;
#sound-dai-cells = <0>;
compatible = "ti,pcm1862";
clocks = <&clks IMX6UL_CLK_SAI1>;
clock-names = "mclk";
};
};
/*Audio CODEC*/
&sai2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai2>;
assigned-clocks = <&clks IMX6UL_CLK_SAI2_SEL>,<&clks IMX6UL_CLK_SAI2>;
assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
assigned-clock-rates = <0>, <12288000>;
fsl,sai-mclk-direction-output;
status = "okay";
};
/*Audio DAC & ADC*/
&sai1 {
#sound-dai-cells= <1>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_sai1>;
assigned-clocks = <&clks IMX6UL_CLK_SAI1_SEL>,<&clks IMX6UL_CLK_SAI1>;
assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
assigned-clock-rates = <0>, <12288000>;
fsl,sai-mclk-direction-output;
status = "okay";
};