Sabre SD Eval Board - Maximum Total Size of MicroSD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sabre SD Eval Board - Maximum Total Size of MicroSD

705 次查看
thomasmorrison
Contributor I

What is the maximum size the supported uboot/linux currently supports and what types

Does the Sabre board SDHS or SDXS?

I am investigating and I have  heard from our distributor that there are issues with some boards?

标记 (2)
0 项奖励
回复
1 回复

621 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Thomas,

What Sabre SD are you using of all?

If you are using IMX6QSABRESD you can find in IMX6Q Reference Manual that uSDHC module conforms to the SD Host Controller Standard Specification version 3.0, so you may check the spec to find out this information.

I am not sure, but I think the theoretical value is 2TB.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复