SW JPEG Codec for i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SW JPEG Codec for i.MX6UL

Jump to solution
782 Views
yuuki
Senior Contributor II

Dear all,

We refer to i.MX_Linux_Rerease_Notes for LinuxBSP of i.MX6UL.

(fsl-yocto-L3.14.52_1.1.0-ga.tar.gz)

In Image codec specification of this document, Encode/Decode of the JPEG is performed by software.

JPEG for i.MX6UL.png

Would you tell me the maximum size that i.MX6UL can support?

Can this support MJPEG, too?

If yes, would you tell me maximum size and fps ?

Best Regards,

Yuuki

Labels (2)
0 Kudos
1 Solution
583 Views
b36401
NXP Employee
NXP Employee

Please note that i.MX6 UL processor has no Image Processing Unit

and all image processing should be performed in the software.

So there are no any special limitations to image size.

As for MJPEG it should be en-/decoded in the software too.

So there is no any special limitations too.

And we have no FPS estimations regarding these codecs.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------                                                            

View solution in original post

0 Kudos
1 Reply
584 Views
b36401
NXP Employee
NXP Employee

Please note that i.MX6 UL processor has no Image Processing Unit

and all image processing should be performed in the software.

So there are no any special limitations to image size.

As for MJPEG it should be en-/decoded in the software too.

So there is no any special limitations too.

And we have no FPS estimations regarding these codecs.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------                                                            

0 Kudos