SPI example for imx8mm running Yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI example for imx8mm running Yocto

2,498 次查看
wdunkley
Contributor III

I've found a couple of documents discussing the SPI bus on the IMX8 chipset running Yocto. However is there any sample code out there that I can use to test out the SPI before trying to integrate it with my other ICs?

 

0 项奖励
回复
4 回复数

2,492 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello wdunkley,

You can view the User guide document for MX8, where you have a an explanation of the SPI driver and how you can use it, also you have the QSPI for booting from M4 core, please got to:

https://www.nxp.com/webapp/Download?colCode=L5.4.24_2.1.0_LINUX_DOCS

 

Regards

 

 

 

0 项奖励
回复

2,488 次查看
wdunkley
Contributor III

Thanks for that, I've read that before and that seems to only explain how to use the SPI to communicate with the flash memory. I'm looking for a little information on using the ECSPI2 on the expansion connector on the evaluation board. Do you know where more information about that is?

Thanks

 

标记 (3)
0 项奖励
回复

2,349 次查看
JunpapaCS
Contributor I

Hello?

Did you find a solution to use the ECSPI2 on the expansion connector on the evaluation board?

I tried to use it with some sample codes but it was failed to be displayed "spidev1.0" under "/dev" fodler.

If you're success it, plz, share the code.

thanks in advance.

0 项奖励
回复

2,482 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

You can read about ECSPI on the reference manual as well, for the connection under the EVK please check the Hardware user guide.

 

0 项奖励
回复