SGTL5000白噪声

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SGTL5000白噪声

640 Views
承王
Contributor I

在IMX536平台上使用SGTL5000播放音乐,播放的歌曲声音基本正确,但是输出总有白噪声,时钟使用的是536处理器输出的时钟,请问这个噪声问题应该怎么解决?电路参考的是官方开发板做的

Labels (1)
0 Kudos
2 Replies

522 Views
igorpadykov
NXP Employee
NXP Employee

Hi 承,

please install latest patches and codecs and try

IMX53_11_09_LINUX_MMCODECS

IMX53_LINUX_1109_BSP_PATCH :

i.MX534: i.MX534 Multimedia Applications Processor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

522 Views
承王
Contributor I

你好:

程序在MCIMX53-START-R开发板上面实验是没有噪声的

--

武汉中原电子

王承

在 2014-04-28 18:27:16,chipexpert <admin@community.freescale.com> 写道:

|

|

|

|

SGTL5000白噪声

reply from chipexpert in i.MX Community - View the full discussion

Hi 承,

please install latest patches and codecs and try

IMX53_11_09_LINUX_MMCODECS http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif

IMX53_LINUX_1109_BSP_PATCH http://www.freescale.com/files/graphic/SECURITYINFOIMAGE.gif :

i.MX534: i.MX534 Multimedia Applications Processor

Reply to this message by replying to this email, or go to the message on Freescale Community

Start a new discussion in i.MX Community by email or at Freescale Community

Following SGTL5000白噪声 in these streams: Inbox

|

|

0 Kudos