SDIO/MMC v2/3 Host Throughput

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDIO/MMC v2/3 Host Throughput

ソリューションへジャンプ
14,875件の閲覧回数
lyfsci
Contributor III

Hi Experts,

What is the maximum effective throughput that could be achieved in the SD/MNC host controller for the various IMX series of processors (IMX 3/5/6) ?

Is there any test suite for EVK or respective factory profiled value for the various platforms along with its associated scenarios ?

1 解決策
4,300件の閲覧回数
art
NXP Employee
NXP Employee

The SD/MMC controller cores of the i.MX3x and i.MX5x series processors are pretty similar. They support the SD/SDIO v.2.0 specification and MMC v.4.2 specification. The Reference Manual documents for these processor series specify the following communication parameters of the SD/MMC controller cores.

— Card bus clock frequency up to 52 MHz

— Up to 416 Mbits/s of data transfer for MMC cards in 8-bit mode

— Up to 200 Mbits/s of data transfer for SD/SDIO cards in 4-bit mode

The SD/MMC controller cores of the i.MX6x series processors support the SD/SDIO v.3.0 specification and MMC v.4.41 specification. The Reference Manual documents for these processor series specify the following communication parameters of the SD/MMC controller cores.

Bus clock frequencies supported are:

- MMC full speed mode (up to 20 MHz)

- MMC high speed mode (up to 52 MHz)

- MMC DDR mode (52MHz both edges)

- SD/SDIO full speed mode (up to 25 MHz)

- SD/SDIO high speed mode (up to 50 MHz)

- SD/SDIO UHS-I mode(up to 208Mhz in SDR mode, up to 50Mhz in DDR mode)

The corresponding data rates are:

- Up to 832 Mbits/s of data transfer for SD/SDIO cards using 4 parallel data lines in SDR(Single Data Rate) mode

- Up to 400 Mbits/s of data transfer for SD/SDIO card using 4 parallel data lines in DDR(Dual Data Rate) mode

- Up to 832 Mbits/s of data transfer for SDXC cards using 4 parallel data lines in SDR(Single Data Rate) mode

- Up to 400 Mbits/s of data transfer for SDXC card using 4 parallel data lines in DDR(Dual Data Rate) mode

- Up to 416 Mbits/s of data transfer for MMC cards using 8 parallel data lines in SDR(Single Data Rate) mode

- Up to 832 Mbits/s of data transfer for MMC cards using 8 parallel data lines in DDR(Dual Data Rate) mode

There are no dedicated test cases for SD/MMC controller cores speed test, since the real data throughput depends on many factors, such as speed of device connected, software overhead etc.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
1,140件の閲覧回数
dfasano
Contributor I

Hi 

I am going to use the Variscite DART6UL board for a project. It has the NXP i.MX 6 Ultralite ARM Cortex-A7 processor. I need to transfer data at 20MB/sec to a SD card.

Does anyone know if that kind of throughput rate is possible with the SD driver running and managing the file structure and writing operation to the SD FLASH memory?

I am concerned about the overhead the driver will impose on the overall data-rate. 

Also, am I correct in assuming the data can be moved under DMA from a parallel input port to the SD bus?

Thanks in advance,

Dan

0 件の賞賛
4,300件の閲覧回数
lyfsci
Contributor III

Hi Artur,

Thanks for the response.

The above mentioned items seems to be the ideal throughput value whereas I look for the actual throughput achieved beyond the signaling constraints in the SoC.

0 件の賞賛
4,301件の閲覧回数
art
NXP Employee
NXP Employee

The SD/MMC controller cores of the i.MX3x and i.MX5x series processors are pretty similar. They support the SD/SDIO v.2.0 specification and MMC v.4.2 specification. The Reference Manual documents for these processor series specify the following communication parameters of the SD/MMC controller cores.

— Card bus clock frequency up to 52 MHz

— Up to 416 Mbits/s of data transfer for MMC cards in 8-bit mode

— Up to 200 Mbits/s of data transfer for SD/SDIO cards in 4-bit mode

The SD/MMC controller cores of the i.MX6x series processors support the SD/SDIO v.3.0 specification and MMC v.4.41 specification. The Reference Manual documents for these processor series specify the following communication parameters of the SD/MMC controller cores.

Bus clock frequencies supported are:

- MMC full speed mode (up to 20 MHz)

- MMC high speed mode (up to 52 MHz)

- MMC DDR mode (52MHz both edges)

- SD/SDIO full speed mode (up to 25 MHz)

- SD/SDIO high speed mode (up to 50 MHz)

- SD/SDIO UHS-I mode(up to 208Mhz in SDR mode, up to 50Mhz in DDR mode)

The corresponding data rates are:

- Up to 832 Mbits/s of data transfer for SD/SDIO cards using 4 parallel data lines in SDR(Single Data Rate) mode

- Up to 400 Mbits/s of data transfer for SD/SDIO card using 4 parallel data lines in DDR(Dual Data Rate) mode

- Up to 832 Mbits/s of data transfer for SDXC cards using 4 parallel data lines in SDR(Single Data Rate) mode

- Up to 400 Mbits/s of data transfer for SDXC card using 4 parallel data lines in DDR(Dual Data Rate) mode

- Up to 416 Mbits/s of data transfer for MMC cards using 8 parallel data lines in SDR(Single Data Rate) mode

- Up to 832 Mbits/s of data transfer for MMC cards using 8 parallel data lines in DDR(Dual Data Rate) mode

There are no dedicated test cases for SD/MMC controller cores speed test, since the real data throughput depends on many factors, such as speed of device connected, software overhead etc.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------