SCM-i.MX 6Dual/6Quad industrial temperature range avilability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCM-i.MX 6Dual/6Quad industrial temperature range avilability

457 Views
ohad
Contributor I

Hi

Please advice if the SCM-i.MX 6Dual/6Quad:

-40°C to +105°C industrial temperature range part is available, if not when will it be ?

Thank you,

Ohad

Labels (1)
0 Kudos
1 Reply

305 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ohad Shaked​,

Yes ,Consumer (0 to +85C) and the Industrial (-40 to +105C). You can go to Single Chip Module-i.MX 6Q|NXP to see the detail.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos