Response on IMX6 solo board is deadly slow

取消
显示结果 
搜索替代 
您的意思是: 

Response on IMX6 solo board is deadly slow

366 次查看
swaraj
Contributor II

Hi,

I got wandboard with IMX6 solo processor on it, it had Ubuntu 11.04 version OS image built on it.

MY IMX6 board is responding very slowly and cannot open GUI at all.

Sometimes I see mmcqd/0 process is consuming too much of CPU.

Can anybody suggest me in resolving this issue.

Thanks,

Swaraj

标签 (3)
0 项奖励
1 回复

206 次查看
SergioSolis
NXP Employee
NXP Employee

I'm not familiar with the wandboard but probably the BSP is not enabled for graphics acceleration, since the CPU is working at full it could be that it is doing all the graphics processing by software rather than hardware.

Have you checked on the wandboard forums to check if their BSP has an update?

0 项奖励