Require DRAM support for i.MX6ULL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Require DRAM support for i.MX6ULL

跳至解决方案
599 次查看
mrudangshelat1
Senior Contributor II

Hi karinavalencia‌ and dgd‌,

In one of the ongoing medical project, we have used i.MX6ULL. And based on datasheet it supports LPDDR2, DDR3, DDR3L. We have used the MCP package of eMMC+LPDDR2 due to form factor constraints in our design. Now the existing MCP package of eMMC+LPDDR2 is EOL. And they have availability only with eMMC+LPDDR3.

Does i.MX6ULL can support LPDDR3 with extra SW effort? If yes, kindly provide the solution.

Else provide the other optional solution. 

Kindly discuss this with your team and provide the answers as soon as possible.

Regards,

Mrudang

标签 (1)
标记 (1)
1 解答
515 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

unfortunately i.MX6ULL does not support LPDDR3, no software workaround available, sorry.

Supported  DDR3(L)/LPDDR2 as described in Chapter 35 Multi Mode DDR Controller (MMDC)

i.MX 6ULL Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
516 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

unfortunately i.MX6ULL does not support LPDDR3, no software workaround available, sorry.

Supported  DDR3(L)/LPDDR2 as described in Chapter 35 Multi Mode DDR Controller (MMDC)

i.MX 6ULL Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

515 次查看
mrudangshelat1
Senior Contributor II

Hi Igor,

thanks for the confirmation.

Mrudang

0 项奖励