Registers can determine of HDCP function?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Registers can determine of HDCP function?

537件の閲覧回数
takashitakahash
Contributor III

Hi community.

Our customer has question ,The i.MX6 has there edition in HDCP function (SCIMX6U5EVM10CC) and function without the version (MCIMX6U6AVM08AC),

Then  Customer would like to determine the HDCP compliant and not support on the software or registers.

Would you tell me there is a register that can determine whether HDCP,

Customer does not determine below registers.

As a confirmed status register

The Product Identification Register1 (12 _ 0003h), both data same as C1h,

Configuration Identification Register0 (12 _ 0004h) both data same as 8 FH also .

ラベル(1)
0 件の賞賛
1 返信

373件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Takashi Takashi,

You should be able to see the HDCP support on the HDMI_PRODUCT_ID1[PRODUCT_ID1] and HDMI_CONFIG0_ID[hdcp] as you mentioned.

It’s strange that you’re seeing the same settings in both parts as the second part should not have the HDCP settings.

I’m investigating regarding this but it’s possible that you may need to open a Service Request to review the marking on these parts. I’ll let you know as soon as I have more information.

For reference to other community users these registers are explained on the Reference Manual (link below).

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf

0 件の賞賛