Regarding PMIC PF3001

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding PMIC PF3001

831 Views
niteshsahay
Contributor III

Hi

I am using PF3001 for my application.I am few question on PF3001:

  • As i am not aware of the sequencing required for my application.Can anyone tell me how can i program the PMIC with my requirement since my application may need n number of iteration to program PF3001 to reach my requirement.
  •  Using I2C how it can be programmed if so any GUI is there or any Source code for the PMIC PF3001 is available. 
  • As mentioned in datasheet PF3001 there are different Vin ranges available for different voltage rails so can i give corresponding input with the different volatge.

Regards

Nitesh 

Labels (1)
0 Kudos
5 Replies

628 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nitesh 

-PF3001 is already preprogrammed so there is no way to

 program the PMIC with your requirements

-  it is programmed similar to PF3000, check i.MX7 bsp sources

- sorry, could you clarify question

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

628 Views
niteshsahay
Contributor III

Hi Igor

Thanks for the reply.

Can i program the sequencing as per my application for PF3001.

Regards

Nitesh

0 Kudos

628 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nitesh 

>Can i program the sequencing as per my application for PF3001.

 

no as PF3001 is already preprogrammed so there is no way to

program the PMIC with another  sequences

Best regards
igor

0 Kudos

628 Views
niteshsahay
Contributor III

Hi Igor

I see one I2C interface on PF3001.

So what is the use of I2C in the application.

Regards

Nitesh

0 Kudos

628 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nitesh 

 

it is used for power management and cpu freq drivers

 

Best regards
igor

0 Kudos