Re: mfgtool imx8mq evk fails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: mfgtool imx8mq evk fails

522件の閲覧回数
dariusz_kazmier
Contributor I

Hi,

I have the same problem.

I want to reinstall my imx8 board bud I have got error:

error.jpg

First installation was done and works correctly, but I have to reinstall system, and now I can't do it?

I use the same port, PC etc.

Where is a problem?

0 件の賞賛
返信
1 返信

480件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   The i.MX8 board should be in Serial (USB) Downloader Boot Mode.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信