RTOS for imx6ul

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RTOS for imx6ul

2,561 次查看
rajprakash
Contributor II

Hi,

I want to debug demo project of freeRTOS for imx6ul.I am using IAR Embedded Workbench (7.60 version ) tool ,J-ling(SEGGER),imx6ul-evk board for my development.I have downloaded the freeRTOS source code from FreeRTOS - Free RTOS Source Code Downloads, the official FreeRTOS zip file release download but my board is not there in the FreeRTOS_V9.0.0rc2->FreeRTOS->demo code so my question is can i customize any demo code for my processor?If possible than please give your idea.

Thanks

Raj

标签 (1)
标记 (2)
0 项奖励
6 回复数

1,218 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Raji

in general one can try to reuse SoloX version, changing headers for other processor

FreeRTOS_BSP_i.MX6SX - Windows installer (REV 1.0.0)

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=FREERTOS_MX6SX_1.0.0_WIN&appType=file1&l...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励

1,218 次查看
rajprakash
Contributor II

Hi igor

Thanks for the reply

I don't know for which headers you are talking about .I open the hello world project but unable to load .out through the JTAG on my imx6ul-evk board because of lots of change require i think to make it work so if you have idea than plz share it.If u have any another way for imx6ul processor than tell me that also.

Thanks

Raj

0 项奖励

1,218 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Raj

one can look at

ARM DS-5 Configuration for i.MX 6UL

~igor

0 项奖励

1,218 次查看
rajprakash
Contributor II

Hi igor

Your's ARM DS-5  Configuration for i.MX 6UL location is not opening.

Thanks

Raj

0 项奖励

1,218 次查看
igorpadykov
NXP Employee
NXP Employee

that link in restricted community area, you can ask local fae to

provide access. Publicly available is AN5229, with the same content

http://cache.nxp.com/files/32bit/doc/app_note/AN5229.pdf

Best regards

igor

0 项奖励

1,218 次查看
rajprakash
Contributor II

Hi igor

I want to know information about freeRTOS related things only.In http://cache.nxp.com/files/32bit/doc/app_note/AN5229.pdf document they are creating projects on ARM DS only no where i found about rtos.I want to go through freeRTOS codes becoz other RTOS is more costly for me.

Thanks

Raj

0 项奖励