RTOS for imx6ul

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTOS for imx6ul

2,544件の閲覧回数
rajprakash
Contributor II

Hi,

I want to debug demo project of freeRTOS for imx6ul.I am using IAR Embedded Workbench (7.60 version ) tool ,J-ling(SEGGER),imx6ul-evk board for my development.I have downloaded the freeRTOS source code from FreeRTOS - Free RTOS Source Code Downloads, the official FreeRTOS zip file release download but my board is not there in the FreeRTOS_V9.0.0rc2->FreeRTOS->demo code so my question is can i customize any demo code for my processor?If possible than please give your idea.

Thanks

Raj

ラベル(1)
タグ(2)
0 件の賞賛
6 返答(返信)

1,201件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raji

in general one can try to reuse SoloX version, changing headers for other processor

FreeRTOS_BSP_i.MX6SX - Windows installer (REV 1.0.0)

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=FREERTOS_MX6SX_1.0.0_WIN&appType=file1&l...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

1,201件の閲覧回数
rajprakash
Contributor II

Hi igor

Thanks for the reply

I don't know for which headers you are talking about .I open the hello world project but unable to load .out through the JTAG on my imx6ul-evk board because of lots of change require i think to make it work so if you have idea than plz share it.If u have any another way for imx6ul processor than tell me that also.

Thanks

Raj

0 件の賞賛

1,201件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raj

one can look at

ARM DS-5 Configuration for i.MX 6UL

~igor

0 件の賞賛

1,201件の閲覧回数
rajprakash
Contributor II

Hi igor

Your's ARM DS-5  Configuration for i.MX 6UL location is not opening.

Thanks

Raj

0 件の賞賛

1,201件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

that link in restricted community area, you can ask local fae to

provide access. Publicly available is AN5229, with the same content

http://cache.nxp.com/files/32bit/doc/app_note/AN5229.pdf

Best regards

igor

0 件の賞賛

1,201件の閲覧回数
rajprakash
Contributor II

Hi igor

I want to know information about freeRTOS related things only.In http://cache.nxp.com/files/32bit/doc/app_note/AN5229.pdf document they are creating projects on ARM DS only no where i found about rtos.I want to go through freeRTOS codes becoz other RTOS is more costly for me.

Thanks

Raj

0 件の賞賛