RT685 Flexcomm design rule.

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

RT685 Flexcomm design rule.

328件の閲覧回数
StephenYeh
Contributor III

Hi Sir

Does the RT685 Flexcomm feature support SPI(MOSI) and GPIO?

 If my system only needs MOSI, and the MISO/SS pin can set to GPIO pin.

 

 

0 件の賞賛
3 返答(返信)

307件の閲覧回数
StephenYeh
Contributor III

Hi Sir,

Thanks.

If I want to share the Flexcomm0 for SPI and I2C @rtos. (It needs re-initial the pin define)

Because our system have many I2C device(same slave address).

Do you recommend this design?

 

0 件の賞賛

301件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

It is possible to share the Flexcomm interface, but as you mentioned you will have to reconfigure the interface to switch between protocols. It will depend on the application if this can affect the desired performance.

Best regards, Daniel.

0 件の賞賛

312件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Flexcomm interface supports the following features:

DanielRuvalcaba_0-1661294656398.png

It does support SPI.

For more information, you can refer to chapter 21 of the UM.

I hope this helps, Daniel.

0 件の賞賛