Pull Up resistor for SDIO interface on i.MX 6SoloX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pull Up resistor for SDIO interface on i.MX 6SoloX

Jump to solution
2,795 Views
andy_kim
Contributor IV

Hello,

I've been checking i.MX 6SoloX Reference schematic and had a query about SDIO interface.

All of SDIO interface have pull up resistor only on SDx_DATA0 and SDx_CMD line.

I don't understand why pull up resistors applied only for two lines except the rest of SDx_DATA lines.

Shouldn't they all SDIO Data lines have pull up resistors?

 

Thanks,

Andy

0 Kudos
1 Solution
2,759 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

You are welcome! Answering your question, the ones used in the design are the minimum required but it does not cause any harm implementing the other pull-ups. 

 

BR,

Ivan.

View solution in original post

0 Kudos
4 Replies
2,780 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

At the booting process normally those pins are required to detect the change of the voltage (NVCC_SD4) switching from 1V8 to 3V1, so please keep them as they are in the design.

 

Hope it helps!

 

BR,

Ivan.

0 Kudos
2,768 Views
andy_kim
Contributor IV

Dear Ivan,

Thanks for your prompt reply.

Then, All of SD1 to SD4 port should be pull up for SDx_DATA0 and SDx_CMD to VCC_SD4? right?

 

Thanks,

Andy

0 Kudos
2,760 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

You are welcome! Answering your question, the ones used in the design are the minimum required but it does not cause any harm implementing the other pull-ups. 

 

BR,

Ivan.

0 Kudos
2,754 Views
andy_kim
Contributor IV

Dear Ivan,

 

Thanks for your confirmation.

 

Andy

0 Kudos