Hi,
We would like to port Ubuntu to IMX6DL board. We are getting the pre-built images only. When we are deploying pre-built images we are not getting all the required files like linux/arch/arm/boot/dts/ doesnot have any dtsi file. some times arch/arm folder itself is not there. it is just booting to Ubuntu that's all.
FTF is referring Yocto Project. But Yocto project is not for Ubuntu. is Ubuntu be built using Yocto project. if So, How.
is there anyway we can get Ubuntu Souce and build it for IMx6DL board. How???
How to get SD card image files (.img/.sdcard) from Source.
HI Srinivasa
ubuntu sources are provided by The leading OS for PC, tablet, phone and cloud | Ubuntu
Re: iMX53 Quick Start Board - The origin of the MicroSD - Ubuntu 10.04 (Lucid) for ARM
for bulding for i.MX6 one can look at below
i.MX6q SABRE Board for Smart Devices - Linux on ARM - eewiki
http://boundarydevices.com/trusty-ubuntu-mx6/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------