Pins assign issue of "Pins for i.MX Version 2.0"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pins assign issue of "Pins for i.MX Version 2.0"

ソリューションへジャンプ
670件の閲覧回数
thanhnhatle
Contributor II

Hi,

In the tool "Pins for i.MX Version 2.0" for MCIMX7DxxVM and MCIMX7SxxVM, the following pins are not matched with datasheet.

Ball Name: DRAM_CAS_B
        datasheet : pin AC14
        Tool: pin AD17


Ball Name: DRAM_DQM1
        datasheet: pin pin AD17
        Tool: pin AC14

Could you please confirm that this is just the tool issue, not the datasheet?
Thank you and wait for your feedback.

ラベル(2)
0 件の賞賛
1 解決策
578件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  The values in the Datasheet are correct.

The ticket  for Pins Tool correction has been already submitted.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
1 返信
579件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello

  The values in the Datasheet are correct.

The ticket  for Pins Tool correction has been already submitted.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛