On Imx8mp linux (5.4.70), is it possible to increase MTU size > 1500 for eth0 ? (fec 30be0000)
I tried to do that and got the below
ifconfig eth1 mtu 2000
SIOCSIFMTU: Invalid argument
I see that various similar posts regarding this such as
https://community.nxp.com/t5/i-MX-Processors/Linux-imx-change-MTU-size-gt-1500/m-p/833837
https://community.nxp.com/t5/i-MX-Processors/How-to-set-jumbo-frame/m-p/1074877, which also refers to a kernel patch https://lore.kernel.org/lkml/1481275255-7650-1-git-send-email-nikita.yoush@cogentembedded.com/
Are these applicable to imx8mp processor as well ? (fec ethernet port, eth0)
Or are there any other patches which are officially supported?
Any guidance on this will be appreciated,