OSS analysation for the library in LTIB Linux BSP for i.MX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OSS analysation for the library in LTIB Linux BSP for i.MX6Solo

Jump to solution
994 Views
yuuki
Senior Contributor II

Dear all,

We use FSL LTIB Linux.
Linux: L3.0.35_4.0.0_ER_SOURCE_BSP

We analyse OSS about our system based on this.
The following library is included in FSL LTIB Linux.
However, the source code of these libraries is not offered.

Do these violate OSS?
If they violate OSS, would you tell me the maker providing these?

Function             Library name           Package
OpenGL           gpu-viv-bin-mx6q    gpu-viv-bin-mx6q-3.0.35-
EGL                 gpu-viv-bin-mx6q    gpu-viv-bin-mx6q-3.0.35-
firmware-imx   firmware-imx            firmware-imx-3.0.35-4.0.
base_libs         base_libs                 base_libs-1.2-1
imx-lib              imx-lib                     imx-lib-3.0.35-4.0.0

Best Regards,
Yuuki

Labels (1)
0 Kudos
1 Solution
693 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
2 Replies
694 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
693 Views
yuuki
Senior Contributor II

Dear all,

We have an additional question.
Would you answer about the following contents?

1)
When we download LTIB Linux, Agreement is displayed.
"FREESCALE SEMICONDUCTOR SOFTWARE LICENSE AGREEMENT"

Do the contents listed in Section 2.Licenses of Agreement apply to all libraries?

2)
We understood that the following library is LGPL license.

# ./ltib -mlistpkgs
-----------------------  ----------------  -----------  -----------  -----------------------------------------
Package                Spec file       Enabled  License   Summary
-----------------------  ----------------  -----------  -----------  -----------------------------------------
base_libs-1.2-1     base_libs      y             LGPL      Base Libraries (from toolchain).

We use this library too.
We think that this library has to be shown a source code.

If our understanding is right, Would you offer the source code of this library?

3)
We use firmware-imx libraries.
This includes Atheros libraries.

We may use following drivers or libraries.
We think that we have to take out these licenses.

Would you tell me how to take out these licenses?

<drivers or libraries>

./ltib/rootfs/lib/modules/3.0.35-2508-g54750ff-MCXV-0x00000104/kernel/
drivers/net/wireless/ath
./ltib/rootfs/lib/modules/3.0.35-2508-g54750ff-MCXV-0x00000104/kernel/
drivers/net/wireless/ath/ath.ko
./ltib/rootfs/lib/modules/3.0.35-2508-g54750ff-MCXV-0x00000104/kernel/
drivers/net/wireless/ath/ath6kl
./ltib/rootfs/lib/modules/3.0.35-2508-g54750ff-MCXV-0x00000104/kernel/
drivers/net/wireless/ath/ath6kl/ath6kl.ko

./ltib/rootfs/lib/firmware/ath6k
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.0/athtcmd_ram.bin
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.0/athwlan.bin.z77
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.0/athwlan.bin
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw1.0/athwlan.bin.z77
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.1.1/athwlan_mobile.bin
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.1.1/athtcmd_ram.bin
./ltib/rootfs/lib/firmware/ath6k/AR6003/hw2.1.1/athwlan.bin
./ltib/rootfs/lib/firmware/ath6k/AR6102/athwlan.bin.z77

Best Regards,
Yuuki

0 Kudos