Not able to hear (using audio port) or speak (using mic port) on imx6qp SabreSD board when a call connection is established

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

Not able to hear (using audio port) or speak (using mic port) on imx6qp SabreSD board when a call connection is established

373件の閲覧回数
sachinarora
Contributor I

Hi,

We are using imx6qp SabreSD eval board (with OREO 8.0) to make a call. We are able to call the other person, but Not able to hear or speak on the mic port and audio-out port.

We are able play an audio file and listen to it using the audio-out port. We are also able to record the audio using the mic port on the kit. But we are not able to hear or speak after the call connection is established.

Kindly help.

 

Regards,

 

Sachin Arora

ラベル(1)
0 件の賞賛
1 返信

261件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

 

Have you installed in the proper way the extended media codecs?

 

Android OS for i.MX Applications Processors | NXP 

Embedded Application Software - miscellaneous

 

For more detail on it, please, refers to the i.MX Android Extended Codec Release Note

 

Best regards,

Diego.

0 件の賞賛