Murata 1MW module with IMX6ULEVK not working

取消
显示结果 
搜索替代 
您的意思是: 

Murata 1MW module with IMX6ULEVK not working

412 次查看
asmaa
Contributor V

Hello All,

I am using Murata 1MW module with imx6 ultralite evaluation kit, I am able to start the bluetooth and connect it to my mobile.

I am following Murata Wi-Fi/BT Solution for i.MX Quick Start Guide (Linux) 6.0 pdf

I want to do file transfer for through put measurement to evaluate it to use it in our product

Build Configuration:
BB_VERSION = "1.36.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ulevk"
DISTRO = "fsl-imx-fb"
DISTRO_VERSION = "4.9-rocko"
TUNE_FEATURES = "arm armv7ve vfp neon callconvention-hard cortexa7"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:9ed1178c87afce997d5a21cadae7461fb6bb48da"
meta-oe
meta-multimedia = "HEAD:352531015014d1957d6444d114f4451e241c4d23"
meta-freescale = "HEAD:a4158e3425a79720ddc4c02e76251d567bdceb51"
meta-freescale-3rdparty = "HEAD:a02324e27f7a7ac630dab616f46a8bad7fe2c071"
meta-freescale-distro = "HEAD:51756d1c2058139c8a21f89b86cfd8007b71b7f0"
meta-bsp
meta-sdk = "HEAD:2f76097309ceb20025af6f0dd853e0f4b641d40a"
meta-browser = "HEAD:2ae23f16309d228ec6f1a25e404b3941115083ee"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:352531015014d1957d6444d114f4451e241c4d23"
meta-qt5 = "HEAD:682ad61c071a9710e9f9d8a32ab1b5f3c14953d1"
meta-murata-wireless = "HEAD:11abc9c7079cc72f454bcd5d95c1584acf311dc1"

I followed the instruction in Bluez5 Spec present at sources/meta-fsl-bsp-release/imx/tools/readme-bluez.txt

When I reach the following step:

6) Copy a file from the board to bluetooth device using the obex transfer.

Note: both obexd and obexctl need to be run from a terminal on the board
instead of from a remote login.

a) Start obex daemon
$ /usr/libexec/bluetooth/obexd

b) On a smart phone, install an obex app such as Bluetooth File Transfer.

c) Start obexctl. Type help to show commands.
$ obexctl

it does not work, it does not connect to Bluetooth File Transfer App. Bluetooth File Transfer app gives error saying the device does not support file transfer.

Regards,

Asma

标记 (2)
0 项奖励
1 回复

286 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we do not support that Murata module. What I suggest you is to go with Murata and ask for the driver and then port it to the Kernel.

I apologize for the inconveniences this could give you.

Best regards,

Diego. 

0 项奖励