MXRT 1050 can work with 1440x240 LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MXRT 1050 can work with 1440x240 LCD

ソリューションへジャンプ
650件の閲覧回数
hiectai
Contributor III

Hello community


I'm trying to figure out if a 1440x240 LCD display can work with an IMXRT 1050.
According to the datasheet of the IMX RT1050, the maximum resolution of LCD is WXGA 1366 x 768. I wonder if H is greater than 1366 or V is greater than 768 it will not be supported right?
Or is the total HxV greater than 1366x768 not supported?


Thank all

ラベル(1)
0 件の賞賛
1 解決策
636件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @hiectai ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) I wonder if H is greater than 1366 or V is greater than 768 it will not be supported right?
-- No, it supports, however, the fresh rate will decrease quickly if the resolution is too big.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
605件の閲覧回数
hiectai
Contributor III

Hi Jeremyzhou

Thanks so much for your answer.

We will connect IMXRT1050 to 1440x240 LCD and evaluate the performance.

Have a nice day.

0 件の賞賛
637件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @hiectai ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) I wonder if H is greater than 1366 or V is greater than 768 it will not be supported right?
-- No, it supports, however, the fresh rate will decrease quickly if the resolution is too big.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------