MX8M :weston-simple-egl failed on debain

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX8M :weston-simple-egl failed on debain

1,060件の閲覧回数
flyalfie
Contributor I

when I process weston-simple-egl.   the message is  "init_egl: Assertion `display->egl.dpy' failed". I saw the code is initEGL faild. it is work on the Yocto. but debain is failed.  please help me. thanks.

0 件の賞賛
5 返答(返信)

942件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Chen,

You should download the latest BSP where weston compositor not failed however you can check with our third party if debian work with it:

https://developer.solid-run.com/knowledge-base/i-mx8m-debian/ 

https://boundarydevices.com/wiki/debian-for-nitrogen8/ 

Regards

0 件の賞賛

942件の閲覧回数
flyalfie
Contributor I

I found out If I run the weston-simple-egl on the debian Stretch,  it is work.  I do not way.  it is impossible run on the debian Buster?

0 件の賞賛

942件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

You should ask to our third party since debian its not supported by nxp.

Regards

0 件の賞賛

942件の閲覧回数
flyalfie
Contributor I

Hello Bio_TICFSL

        thanks  for your answer.   I try to downland debian-buster-sdhc img.  bug it can not boot from MMC

 U-Boot SPL 2018.11-08002-g8e521a3525 (Nov 20 2019 - 16:49:56 +0000)
PMIC: PFUZE100 ID=0x10
Training FAILED
Training FAILED
Training FAILED
Normal Boot
Trying to boot from MMC2
MMC Device 1 not found
spl: could not find mmc device 1. error: -19
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ##

0 件の賞賛

942件の閲覧回数
flyalfie
Contributor I

I am try to boot loader for SD card. but it is no work

0 件の賞賛