[MX25][MMC] mmc esdhc very slow r/w speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[MX25][MMC] mmc esdhc very slow r/w speed

659 Views
maximkochetkov
Contributor II

Hi!
I have the same problem as:
http://lists.infradead.org/pipermail/linux-arm-kernel/2012-March/091529.html
Read/write speed of SDHC card is very slow.
Kernel 2.6.35 from Freescale works with a excellent SDHC performance.
Mainline kernels from 3.17 to 4.9.5 works very slow with SDHC.
Is there any solutions about this problem?

Labels (2)
0 Kudos
3 Replies

553 Views
igorpadykov
NXP Employee
NXP Employee

Hi Maxim

there are number of eSDHC errata which should be carefully

implemented to achieve good performance

http://www.freescale.com/files/dsp/doc/errata/IMX25CE.pdf 

Unfortunately there is no nxp(fsl) i.MX25 support for new kernels

and you should implement this yourself or consider some mss services

like Pro-Support www.nxp.com/prosupport .

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

553 Views
maximkochetkov
Contributor II

What is the latest nxp (fsl) kernel version and where can I get it?

0 Kudos

553 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos