MMC THGBM4G4D1HBAIR on IMX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMC THGBM4G4D1HBAIR on IMX53

Jump to solution
835 Views
cristiansicilia
Contributor III

Hello *,

I have an IMX53 with an MMC THGBM4G4D1HBAIR, but seems that linux can't read the Card ID.

The Layout

MMC-IMX53.png

The MMC_RST and MMC_CMD are connected on PATA_IORDY and NPATA_RESET_B respectivelly.

In my board code have:

// IOMUX MMC

MX53_PAD_PATA_DATA8__ESDHC3_DAT0,

MX53_PAD_PATA_DATA9__ESDHC3_DAT1,

MX53_PAD_PATA_DATA10__ESDHC3_DAT2,

MX53_PAD_PATA_DATA11__ESDHC3_DAT3,

MX53_PAD_PATA_DATA0__ESDHC3_DAT4,

MX53_PAD_PATA_DATA1__ESDHC3_DAT5,

MX53_PAD_PATA_DATA2__ESDHC3_DAT6,

MX53_PAD_PATA_DATA3__ESDHC3_DAT7,

MX53_PAD_PATA_IORDY__ESDHC3_CLK,

MX53_PAD_PATA_RESET_B__ESDHC3_CMD,

MX53_PAD_PATA_DA_0__ESDHC3_RST,

static struct mxc_mmc_platform_data mmc3_data = {

  .ocr_mask = MMC_VDD_31_32,

  .caps = MMC_CAP_NONREMOVABLE | MMC_CAP_8_BIT_DATA | MMC_CAP_DATA_DDR,

  .min_clk = 400000,

  .max_clk = 50000000,

  .card_fixed = 1,

  .card_inserted_state = 0,

  .clock_mmc = "esdhc_clk",

  .power_mmc = NULL,

};

  mxc_register_device(&mxc_iim_device, &iim_data);

  //mxc_register_device(&mxc_pwm2_device, NULL);

  mxc_register_device(&mxcsdhc1_device, &mmc1_data); // SDCARD this work good

  mxc_register_device(&mxcsdhc3_device, &mmc3_data); // MMC not work

  mxc_register_device(&mxc_ssi1_device, NULL);

  mxc_register_device(&mxc_ssi2_device, NULL);    //

The kernel log oututp with MMC debug enabled say:

Jan  2 00:25:19 nsip user.warn kernel: .

Jan  2 00:25:19 nsip user.debug kernel: mmc1: starting CMD2 arg 00000000 flags 00000067

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_send_command()]: sdhci_send_command 0x2 is starting...

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_send_command()]: Complete sending cmd, transfer mode would be 0x2090000.

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_irq()]: *** mmc1 got interrupt: 0x00010001

Jan  2 00:25:19 nsip user.debug kernel: mmc1: req failed (CMD2): -110, retrying...

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_send_command()]: sdhci_send_command 0x2 is starting...

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_send_command()]: Complete sending cmd, transfer mode would be 0x2090000.

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_irq()]: *** mmc1 got interrupt: 0x00010001

Jan  2 00:25:19 nsip user.debug kernel: mmc1: req failed (CMD2): -110, retrying...

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_send_command()]: sdhci_send_command 0x2 is starting...

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_send_command()]: Complete sending cmd, transfer mode would be 0x2090000.

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_irq()]: *** mmc1 got interrupt: 0x00010001

Jan  2 00:25:19 nsip user.debug kernel: mmc1: req failed (CMD2): -110, retrying...

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_send_command()]: sdhci_send_command 0x2 is starting...

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_send_command()]: Complete sending cmd, transfer mode would be 0x2090000.

Jan  2 00:25:19 nsip user.debug kernel: mxsdhci [sdhci_irq()]: *** mmc1 got interrupt: 0x00010001

Jan  2 00:25:19 nsip user.debug kernel: mmc1: req done (CMD2): -110: 00000000 00000000 00000000 00000000

Seems that the function mmc_all_send_cid fail for timeout (err -110).

Any Idea?

Tags (2)
0 Kudos
1 Solution
580 Views
igorpadykov
NXP Employee
NXP Employee

Hi Cristian

had you set SION bit for mmc pad iomux settings ?

One can try to test mmc signals with oscilloscope using simple OBDS

mmc_test.c (read mmc ID)

On-Board Diagnostic Suit for the i.MX53 Quick Start Board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
580 Views
cristiansicilia
Contributor III

Hello Igorpaykov,

thank's for reply.

The iomux settings:

  1. // IOMUX MMC 
  2. MX53_PAD_PATA_DATA8__ESDHC3_DAT0, 
  3. MX53_PAD_PATA_DATA9__ESDHC3_DAT1, 
  4. MX53_PAD_PATA_DATA10__ESDHC3_DAT2, 
  5. MX53_PAD_PATA_DATA11__ESDHC3_DAT3, 
  6. MX53_PAD_PATA_DATA0__ESDHC3_DAT4, 
  7. MX53_PAD_PATA_DATA1__ESDHC3_DAT5, 
  8. MX53_PAD_PATA_DATA2__ESDHC3_DAT6, 
  9. MX53_PAD_PATA_DATA3__ESDHC3_DAT7, 
  10. MX53_PAD_PATA_IORDY__ESDHC3_CLK, 
  11. MX53_PAD_PATA_RESET_B__ESDHC3_CMD, 
  12. MX53_PAD_PATA_DA_0__ESDHC3_RST, 

was not call, so I simply don't apply this settings (as your indication).

Really thank's for your suggestion!!

0 Kudos
581 Views
igorpadykov
NXP Employee
NXP Employee

Hi Cristian

had you set SION bit for mmc pad iomux settings ?

One can try to test mmc signals with oscilloscope using simple OBDS

mmc_test.c (read mmc ID)

On-Board Diagnostic Suit for the i.MX53 Quick Start Board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos