MIPI CSI-2 camera doesn't receive the first frame

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIPI CSI-2 camera doesn't receive the first frame

938 次查看
titusstalin
Contributor V

Hello Experts,

I have connected our MIPI CSI-2 camera to i.MX6 board.

And it not capturing the first frame everytime, camera sends 10 frames and i.MX receives 9frames only.

What could be the problem ?

MIPI CSI-2 i.MX host is ignoring the first frame due to avoid the unsynced frames ??

标签 (5)
标记 (1)
2 回复数

780 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Titus

you are right, if frame is started capturing in the middle,

it can be ignored, so capture happens after first successful frame sync

with second frame.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

780 次查看
titusstalin
Contributor V

Thanks Igor for your confirmation.

0 项奖励
回复