MFG tool in i.MX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFG tool in i.MX8M

Jump to solution
3,502 Views
yashavanthashet
Contributor V

Hi,

I'm using i.MX8M custom board.

Here MFG tool is failing in below place. Using Type C as OTG.

The available udc:
/sys/class/udc/38100000.dwc3
[    5.940293] Mass Storage Function, version: 2009/09/11
[    5.945456] LUN: removable file: (no medium)
MFG tool will use 1st udc:38100000.dwc3
/linuxrc: line 53: echo: write error: Device or resource busy
Starting UTP
uuc 0.5 [built Mar 12 2018 12:14:52]
UTP: Waiting for device to appear

It is not moving further after below prints.

In kernel I have enabled

CONFIG_FSL_UTP

CONFIG_USB_CONFIGFS_MASS_STORAGE

CONFIG_MASS_STORAGE,

Is there any other macros needs to be enabled in Linux kernel? Whether any changes required in Uboot to be done?

MFG boot log added.

Thanks in advance.

Regards,

Yashavantha

1 Solution
2,776 Views
yashavanthashet
Contributor V

Hi,

Thank you for your support.

MFG tool is working with windows10 OS, but not with windows 7.

Regards,

Yashvantha

View solution in original post

0 Kudos
7 Replies
2,776 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yashavantha

one can try to rebuild mfg tool firmware (files in mfg tool ../firmware folder) with new ones

and using results from ddr test, follow Chapter 4 How to bring up a new MX8M board MX8M_DDR_Tool_User_Guide.docx
i.MX 8M DDR Tool Release 
For rebuilding please use sect.6.2 Manufacturing Tool, MFGTool  attached Yocto Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
2,776 Views
yashavanthashet
Contributor V

Hi Igor,

After updating properly config file, it is moving little further, But now hanging at "Jumping to OS image".

I have attached the MFG log here.

Kindly provide your inputs regarding this.

Thanks and Regards,

Yashavanha

0 Kudos
2,776 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yashavantha

 

please try to rebuild mfg tool firmware (files in mfg tool ../firmware folder) with new ones

and using results from ddr test, follow Chapter 4 How to bring up a new MX8M board MX8M_DDR_Tool_User_Guide.docx
i.MX 8M DDR Tool Release 
For rebuilding please use sect.6.2 Manufacturing Tool, MFGTool  attached Yocto Guide

 

Best regards
igor

0 Kudos
2,776 Views
yashavanthashet
Contributor V

Hi Igor,

I am not using the default binaries in firmware folder, I have already build with updated DDR changes and using the same binaries in firmware folder too.

And I'm doing standalone compilation of u-boot and kernel source code, not through yocto.

Thanks and Regards,

Yashavantha

0 Kudos
2,776 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yashavantha

suggest to try procedure using yocto, as this is nxp officially supported option.

For non-yocto options one can try to get help with  Professional Services

NXP Professional Services|NXP 

Best regards
igor

2,776 Views
yashavanthashet
Contributor V

Hi Igor,

Thank you.

But is there anything can you say after looking at MfgTool.log which I have attached above??

Thanks and Regards,

Yashavantha

0 Kudos
2,777 Views
yashavanthashet
Contributor V

Hi,

Thank you for your support.

MFG tool is working with windows10 OS, but not with windows 7.

Regards,

Yashvantha

0 Kudos