MCIMX8QM-CPU Dual Display touch issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCIMX8QM-CPU Dual Display touch issue

1,032 次查看
SL239
Contributor II

I am running Android Automotive on the iMX8QM board.

I have two displays hooked up to LVDS0_CH0 and LVDS1_CH0. The display LVDS0_CH0 has the usb-c connected for touch.

I am running imx_automotive_11.0.0_2.3.0 in the mek_8q_car_userdebug build.

My issue is when I connect one display to the LVDS0_CH0 channel the Automotive Launcher and my touch works perfectly fine. But When I connect the second display to LVDS1_CH0 the Instrument Cluster and the Automotive Launcher come up just fine but then all of the touch points on the first screen are counted only on the second screen. (So touches on the LVDS0_CH0 monitor effect only the LVDS1_CH0 monitor.

Has anyone experienced this issue before?

Thanks.

0 项奖励
回复
2 回复数

746 次查看
PunitTeksun
Contributor I

Hello,

Do you know how can we change the primary display? I have also connected two displays and both displays are working fine. 

1st display : 1920X720 (I need to make this display as primary display)

2nd Display : 1280X800 (This is getting registered as a primary display)

Can you let me know where i need to do the modification. 

0 项奖励
回复

959 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Please check how the binding of the display and the input has been defined.

You may refer to the User's guide chapter 8.3.3.1 Binding the display port with the input port.

Best regards,
Aldo.

0 项奖励
回复