The IMXVIRTUG guide tells us to run the command:
"jailhouse enable imx8mq-veth.cell"
And after downloading multiple version of the imx8mq images (up to LF_v5.15.32-2.0.0_images_IMX8MQEVK), still not found it.
Is it a real thing, or renamed, or ???
解決済! 解決策の投稿を見る。
Hello,
That Manual is for L4.14.98_2.0.0_ga you need to download to follow that guide:
Regards
The problem with that answer is the L4.14.98_2.0.0_ga_images_MX8MQEVK does not have the jailhouse binary (in the sdcard image - or the tarball inside it). The documents presume that you are building the corresponding yocto.
So the best thing to tell people is, "The IMXVIRTUG is out of date. Please download the latest image (LF_v5.15.32-2.0.0_images_IMX8MQEVK.zip) and ignore the references to imx8mq-veth.cell as the drivers are built in now). Also you need to have a root filesystem on the eMMC device or the demo will not work, Once you have the eMMC loaded with an image:
boot to a prompt :
run jh_mmcboot
Then in Linux prompt : (this assumes your linux "inmate" image is on mmcblk2p2
modprobe jailhouse
jailhouse enable /usr/share/jailhouse/cells/imx8mq.cell
export PATH=$PATH:/usr/share/jailhouse/tools
jailhouse cell linux /usr/share/jailhouse/cells/imx8mq-linux-demo.cell /run/media/mmcblk1p1/Image -d /run/media/mmcblk1p1/imx8mq-evk-inmate.dtb -c "clk_ignore_unused console=ttymxc1,115200 earlycon=ec_imx6q,0x30860000,115200 root=/dev/mmcblk2p2 rootwait rw"
The usb console cable has two consoles on it (on your PC, /dev/ttyUSB0 and /dev/ttyUSB1 - if you have no other serial consoles hooked up) and the jailhouse console will be on the second one, and main console is on the first (root).
If successful, your inmate will have set up a virtual Ethernet interface, and can ssh between them once you identify the addresses of the root and the inmate.
So I am to infer that imx8mq-veth.cell is obsolete for 5.15 image for the imx8mq EVK?
I did get it working and the Ethernet worked between the root and the inmate.
Hello,
That Manual is for L4.14.98_2.0.0_ga you need to download to follow that guide:
Regards