Hi all,
Is SN65LVDS315 (MIPI CSI-1) compatible with our i.MX8MMini MIPI CSI-2 interface ?
CSI-2 extends CSI-1 with multiple lanes, but both standards use the same D-PHY layer.
According to the following thread, it can't connect with i.MX6 and SN65LVDS315 due to the difference of standard.
https://community.nxp.com/docs/DOC-96385
We guess that it's same as i.MX8MMini. Am I correct ?
Ko-hey
已解决! 转到解答。
HI Ko-Hey,
Yes, the CSI-2 interface is not compatible with CSI-1 devices and cannot use SN65LVDS315 for CSI-2 Interface.
Regards,
Mrudang