Is it possible to configure Slew Rate of HDMI or LVDS pins on i.MX6DL?

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

Is it possible to configure Slew Rate of HDMI or LVDS pins on i.MX6DL?

ソリューションへジャンプ
572件の閲覧回数
andrejakostic
Contributor II

I'd just like to confirm if the slew rate and drive strength are configurable for the LVDS (LVDS0 CLK p/n and Data 0/1/2 p/n) and HDMI(TX CLK p/n and TX Data 0/1/2 p/n) pins on the i.MX6DL.


As far as I can understand from reading the reference manual, the LVDS pins have fixed configuration, which cannot be changed in the software, and the slew rate of the HDMI pins cannot be configured in software, but the drive strength is configurable using the procedure explained in the chapter 35.8 of the reference manual.

So is the above correct?

ラベル(1)
1 解決策
455件の閲覧回数
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Andreja

I think this is correct understanding.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
456件の閲覧回数
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Andreja

I think this is correct understanding.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------