Is i.MX6/7 DDR Stress Test Tool V2.70 available for 32-bit OS ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is i.MX6/7 DDR Stress Test Tool V2.70 available for 32-bit OS ?

444 Views
govarthanamkris
Contributor I

I would like to if there is a 32-bit version of the Stress Test Tool available.

0 Kudos
1 Reply

362 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The DDR Stress Test Tool does not work under 32-bit (say, Win XP), sorry.

No special tool version for it.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos