Integrate 88W8997 to iMX8MPlus L5.4.70.2.3.0 but compiler fail.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integrate 88W8997 to iMX8MPlus L5.4.70.2.3.0 but compiler fail.

Jump to solution
929 Views
charleshuang
Senior Contributor II

Hi NXP 

We try to Integrate 88W8997 to iMX8MPlus - Yocto3.0 -L5.4.70.2.3.0.

The wifi 88w8997 version

 PCIE-WLAN-UART-BT-8997-U16-X86-W16.68.10.p16-16.26.10.p16-C4X16640_V4-GPL.zip

But try to compiler get error.  Do you have any idea ?

Where I can download the 8997 aarch64 linux driver?

fail.jpg

 

Labels (1)
0 Kudos
1 Solution
2 Replies
903 Views
charleshuang
Senior Contributor II

Hi NXP

Thanks

The driver is ready and test it.  The result is pass.

0 Kudos