Hi NXP
We try to Integrate 88W8997 to iMX8MPlus - Yocto3.0 -L5.4.70.2.3.0.
The wifi 88w8997 version
PCIE-WLAN-UART-BT-8997-U16-X86-W16.68.10.p16-16.26.10.p16-C4X16640_V4-GPL.zip
But try to compiler get error. Do you have any idea ?
Where I can download the 8997 aarch64 linux driver?
Solved! Go to Solution.
Hi Charles
one can look at sect.4.13.4 Source Code Structure i.MX Linux Reference Manual
https://source.codeaurora.org/external/imx/mwifiex/tree/
Best regards
igor
Hi Charles
one can look at sect.4.13.4 Source Code Structure i.MX Linux Reference Manual
https://source.codeaurora.org/external/imx/mwifiex/tree/
Best regards
igor
Hi NXP
Thanks
The driver is ready and test it. The result is pass.