Hi Sir/Mam,
I am using I.mx6ull processor(EVK) in that default camera data lines used(CSI_DATA00 to CSI_DATA07) instead of that pins can i use alternative pins (CSI_DATA6,CSI_DATA7,CSI_DATA8,CSI_DATA9,CSI_DATA16,CSI_DATA17,CSI_DATA18,CSI_DATA19) ?
Hi prabhu
csi pin usage is described in sect.19.4 Principles of Operation i.MX6UL Reference Manual
and can not be changed.
http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
Thanks for your reply.
Hi igor,
Currently i am using UART1_TX_DATA & UART1_RX_DATA as Debug UART instead of that can i use alternative pins(UART2_TX_DATA & UART2_RX_DATA, UART3_TX_DATA & UART3_RX_DATA, UART4_TX_DATA & UART4_RX_DATA, UART5_TX_DATA & UART5_RX_DATA) any of this for Debug UART ?