IMX8QM - OTA Update: Combined 2 differential update into single differential update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM - OTA Update: Combined 2 differential update into single differential update

847 Views
vinothkumars
Senior Contributor IV

Hi All,

 

Is there possible to combine two differential OTA into single Differential OTA.

If it possible let me provide the steps.

Regards,
Vinothkumar Sekar
0 Kudos
3 Replies

798 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @vinothkumars,

I am including below my reply to your query,

[Q] Is there possible to combine two differential OTA into a single Differential OTA?

[A]
Please refer to Android User's Guide, sect. 7.1.3 Building an incremental update package.
In the first step, you can generate the incremental update package from the first two packages and get the resultant package.
Then do the same process with other packages with the resultant package and generate the final update package.

 

Thanks & Regards,
Dhruvit.

0 Kudos

781 Views
vinothkumars
Senior Contributor IV
Thank you, Will check
Regards,
Vinothkumar Sekar
0 Kudos

750 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @vinothkumars,

 

Waiting for your response.

 

Thanks & Regards,

Dhruvit Vasavada

0 Kudos