IMX8QM Dual Display (LCD and HDMI)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QM Dual Display (LCD and HDMI)

1,402 Views
prashanthkumar
Contributor II

Dear All,

LCD and HDMI are working individually.

How to configure the dual display support in imx8qm - "imx-yocto-L4.14.78_1.0.0_ga" release.

1. LCD - 1080x1920 (MIPI-DSI1)

2. HDMI.

Regards,

Prashanth Kumar K

0 Kudos
2 Replies

830 Views
prashanthkumar
Contributor II

Dear Joan Xie,

We are checked “fsl-imx8qm-mek.dtsi” file for Dual display, in that Two LVDS/MIPI-DSI Displays are supported, each LVDS/MIPI-DSI is from different Display controller.


In our case both the displays (Native HDMI and MIPI-DSI-1) are from to single Display controller (DPU).
Please share the changes for Dual Display support using single Display controller (DPU).

Best Regards,

Prashanth Kumar K

0 Kudos

830 Views
joanxie
NXP TechSupport
NXP TechSupport

I haven't imx8 board to test for you , but you can try to use fsl-imx8qm-mek.dtb, which should support dual display.

0 Kudos