Dear Experts,
I built the isp-imx 4.2.2.11.0 in Partial/Debug mode :
$ ./build-all-isp.sh debug
BUILD_TYPE: debug
BUILD: partial
Partial build --------------------->
Debug build --------------------->
However, when executing the run.sh script on non-Yocto image (I'm using Buildroot based image) :
Starting isp_media_server with configuration file CAMERA0
./isp_media_server: symbol lookup error: /usr/lib/libbufsync_ctrl.so: undefined symbol: trace
Has anyone ever struggled with similar situation, please ?
Thanks in advance and best regards,
Khang
解決済! 解決策の投稿を見る。
I got information that this source code isn't released to customer full version, only partial version
I found libbusfync_ctrl folder is under isp-imx-xxx/units, how about building the source code again?
"./build-all-isp.sh Release Full"
Dear @joanxie,
I also mentioned the build combination that you proposed here : https://community.nxp.com/t5/i-MX-Processors/ISP-working-in-i-MX8M-Plus/m-p/1246838
To repeat, ./build-all-isp.sh Release Full felt back to Partial build (i.e. ./build-all-isp.sh Release Partial or./build-all-isp.sh Release simply, see the log) since Full is NOT a correct option but full, however this later does not work due to private resource (aaa) :
./build-all-isp.sh Release Full BUILD_TYPE: release BUILD: Full Partial build ---------------------> Release build --------------------->
Best regards,
Khang
I got information that this source code isn't released to customer full version, only partial version